Note:
- File objects can only be modified by replacing the entire file.
- File objects must be written sequentially.
Dynamically Creatable: No
Dynamically Deletable: No
Property Name |
Required |
Optional |
Proprietary |
Property ID |
Data Type |
Writable |
Range |
---|---|---|---|---|---|---|---|
OBJECT_NAME |
X |
77 |
|||||
FILE_TYPE |
X |
43 |
|||||
MODIFICATION_DATE |
X |
71 |
|||||
READ_ONLY |
X |
99 |
|||||
FILE_ACCESS_METHOD |
X |
41 |
|||||
ARCHIVE |
X |
13 |
X |
||||
FILE_SIZE 1 |
X |
42 |
X |
||||
DESCRIPTION |
X |
28 |
X |
40 characters max |
|||
ITEM_REFERENCE |
X |
32527 |
Character String |
||||
USER_NAME |
X |
2390 |
Character String |
||||
STATUS |
X |
512 |
Enumerated |
||||
ENABLED |
X |
673 |
Boolean |
X |
|||
EXECUTION_PRIORITY |
X |
2197 |
Enumerated |
X |
0–3 |
||
OBJECT_CATEGORY |
X |
908 |
Enumerated |
X |
0–249 |
||
ALARM_STATE |
X |
1006 |
Enumerated |
||||
MAX_FILE_SIZE |
X |
3380 |
Unsigned |
1 Can write zero (0) to file size but
arbitrary truncation or expansion is not
supported.