The following is a list of the standard object types as defined by
ASHRAE that are currently supported in these products. See the appropriate supported
object type section in this document for details.
Table 1. MS-IOM2723-0 - Supported Object Types
Device |
Analog Output |
File |
Analog Value |
Multistate Value |
Binary Input |
Analog Input |
Binary Value |
Network Port |
Table 2. MS-IOM3723-0 - Supported Object Types
Device |
Binary Input |
File |
Binary Value |
Multistate Value |
Accumulator |
Network Port |
Table 3. MS-IOM3733-0 - Supported Object Types
Device |
Binary Input |
File |
Binary Output |
Multistate Value |
Binary Value |
Accumulator |
Network Port |