Networking Options - BCPro - Facility Explorer - LIT-12012986 - CH-PCX2723-0 - CH-PCX3723-0 - CH-PCX3733-0 - Field Device - FX-PCX17 Expansion Input/Output Module - FX-PCX27 Expansion Input/Output Module - FX-PCX37 Expansion Input/Output Module - FX-PCX47 Expansion Input/Output Module

Programmable Controller Expansion Input/Output Module (PCX) Series Protocol Implementation Conformance Statement

Product
Controls > Input/Output Controls > FX-PCX47 Expansion Input/Output Module
Controls > Input/Output Controls > FX-PCX17 Expansion Input/Output Module
Controls > Input/Output Controls > FX-PCX27 Expansion Input/Output Module
Controls > Input/Output Controls > FX-PCX37 Expansion Input/Output Module
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12012986
Revision date
2020-11-11

Router, Clause 6

   

Annex H, BACnet Tunneling Router over IP

   

BACnet/IP Broadcast Management Device (BBMD)

   
 

Does the BBMD support registrations by Foreign Devices?

Yes

No