Network Security Options - BCPro - Facility Explorer - LIT-12012986 - CH-PCX2723-0 - CH-PCX3723-0 - CH-PCX3733-0 - Field Device - FX-PCX17 Expansion Input/Output Module - FX-PCX27 Expansion Input/Output Module - FX-PCX37 Expansion Input/Output Module - FX-PCX47 Expansion Input/Output Module

Programmable Controller Expansion Input/Output Module (PCX) Series Protocol Implementation Conformance Statement

Brand
BCPro
Facility Explorer
Product name
FX-PCX17 Expansion Input/Output Module
FX-PCX27 Expansion Input/Output Module
FX-PCX37 Expansion Input/Output Module
FX-PCX47 Expansion Input/Output Module
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12012986
Revision date
2020-11-11
Language
English

Non-secure Device - is capable of operating without BACnet Network Security

Secure Device - is capable of using BACnet Network Security (NS-SD BIBB)

 

Multiple Application-Specific Keys:

 

Supports encryption (NS-ED BIBB)

 

Key Server (NS-KS BIBB)