Document Introduction - BCPro - Facility Explorer - LIT-12012986 - CH-PCX2723-0 - CH-PCX3723-0 - CH-PCX3733-0 - Field Device - FX-PCX17 Expansion Input/Output Module - FX-PCX27 Expansion Input/Output Module - FX-PCX37 Expansion Input/Output Module - FX-PCX47 Expansion Input/Output Module

Programmable Controller Expansion Input/Output Module (PCX) Series Protocol Implementation Conformance Statement

Brand
BCPro
Facility Explorer
Product name
FX-PCX17 Expansion Input/Output Module
FX-PCX27 Expansion Input/Output Module
FX-PCX37 Expansion Input/Output Module
FX-PCX47 Expansion Input/Output Module
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12012986
Revision date
2020-11-11
Language
English

This document contains the Protocol Implementation Conformance Statement (PICS) and BACnet® Interoperability Building Blocks (BIBBs) for the PCX2723-0, PCX3723-0, and PCX3733-0 Controllers as required by the ANSI/ASHRAE Standard 135 for BACnet protocol.

The PICS is a written document created by the manufacturer of a device to identify the particular options specified in the BACnet standard and implemented in the device.

BIBBs are collections of one or more BACnet services. This document includes a listing of the BIBBs currently supported by the PCX2723-0, PCX3723-0, and PCX3733-0 .