Character Sets Supported - BCPro - Facility Explorer - LIT-12012986 - CH-PCX2723-0 - CH-PCX3723-0 - CH-PCX3733-0 - Field Device - FX-PCX17 Expansion Input/Output Module - FX-PCX27 Expansion Input/Output Module - FX-PCX37 Expansion Input/Output Module - FX-PCX47 Expansion Input/Output Module

Programmable Controller Expansion Input/Output Module (PCX) Series Protocol Implementation Conformance Statement

Product
Controls > Input/Output Controls > FX-PCX47 Expansion Input/Output Module
Controls > Input/Output Controls > FX-PCX17 Expansion Input/Output Module
Controls > Input/Output Controls > FX-PCX27 Expansion Input/Output Module
Controls > Input/Output Controls > FX-PCX37 Expansion Input/Output Module
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12012986
Revision date
2020-11-11

Indicating support for multiple character sets does not imply that they can all be supported simultaneously.

IBM®/Microsoft® Double-Byte Character Set (DBCS)

ISO 10646 Universal Character Set-2 (UCS-2)

ISO 10646 (UCS-4)

ISO10646 (UTF-8)

ISO 8859-1

Japanese Industrial Standard (JIS) X 0208