BACnet Standardized Device Profile (Annex L) - BCPro - Facility Explorer - LIT-12012986 - CH-PCX2723-0 - CH-PCX3723-0 - CH-PCX3733-0 - Field Device - FX-PCX17 Expansion Input/Output Module - FX-PCX27 Expansion Input/Output Module - FX-PCX37 Expansion Input/Output Module - FX-PCX47 Expansion Input/Output Module

Programmable Controller Expansion Input/Output Module (PCX) Series Protocol Implementation Conformance Statement

Brand
BCPro
Facility Explorer
Product name
FX-PCX17 Expansion Input/Output Module
FX-PCX27 Expansion Input/Output Module
FX-PCX37 Expansion Input/Output Module
FX-PCX47 Expansion Input/Output Module
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12012986
Revision date
2020-11-11
Language
English

BACnet Operator Workstation (B-OWS)

BACnet Advanced Operator Workstation (B-AWS)

BACnet Operator Display (B-OD)

BACnet Building Controller (B-BC)

BACnet Advanced Application Controller (B-AAC)

BACnet Application Specific Controller (B-ASC)

BACnet Smart Sensor (B-SS)

BACnet Smart Actuator (B-SA)

BACnet Other (B-Other)