BACnet Interoperability Building Blocks (BIBBs) (Annex K) - BCPro - Facility Explorer - LIT-12012986 - CH-PCX2723-0 - CH-PCX3723-0 - CH-PCX3733-0 - Field Device - FX-PCX17 Expansion Input/Output Module - FX-PCX27 Expansion Input/Output Module - FX-PCX37 Expansion Input/Output Module - FX-PCX47 Expansion Input/Output Module

Programmable Controller Expansion Input/Output Module (PCX) Series Protocol Implementation Conformance Statement

Brand
BCPro
Facility Explorer
Product name
FX-PCX17 Expansion Input/Output Module
FX-PCX27 Expansion Input/Output Module
FX-PCX37 Expansion Input/Output Module
FX-PCX47 Expansion Input/Output Module
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12012986
Revision date
2020-11-11
Language
English

The following table lists all BIBBs that are supported. The table is divided into BIBBs required for the Controller (B-SA) profile, followed by additional BIBBs that are supported, but not required, for the profile.

Table 1. BACnet B-SA BIBBs Support

BIBB Name (A = Initiates and B = Executes)

Designation

Required for B-SA Profile

Data Sharing - Read Property - B

DS-RP-B

Data Sharing - Write Property - B

DS-WP-B

Device Management - Dynamic Device Binding - B

DM-DDB-B

Device Management - Dynamic Object Binding - B

DM-DOB-B

Not Required for B-SA Profile

Data Sharing - Read Property Multiple - B

DS-RPM-B

Data Sharing - Write Property Multiple - B

DS-WPM-B

Data Sharing - Change Of Value - B

DS-COV-B

Data Sharing - Change Of Value Property - B

DS-COVP-B

Data Sharing - Change Of Value Unsubscribed - B

DS-COVU-B

Executes ReadRange Executes ReadRange

Device Management - Time Synchronization - B

DM-TS-B

Device Management - UTC Time Synchronization - B

DM-UTC-B

Device Management - Device Communication Control - B

DM-DCC-B

Device Management - Reinitialize Device - B

DM-RD-B

Device Management - Restart - B

DM-R-B

Device Management - List Manipulation - B

DM-LM-B