A set of Johnson Controls termination diagrams provides details for wiring inputs and outputs. See the figures in this section for the applicable termination diagrams.
Type of device |
Type of Input/Output |
Termination diagrams |
---|---|---|
Dry Contact (Binary Input) |
BI |
|
Incremental Control to Actuator (Switch Low, Externally Sourced) |
BO |
|
24 VAC Binary Output (Switch Low, Externally Sourced) |
BO |
|
24 VAC Binary Output (Switch High, Externally Sourced) |
BO |
|
Incremental Control to Actuator (Switch High, Externally Sourced) |
BO |