Use the following figure to estimate the maximum cable length relative to the wire size and the load current (in mA) when wiring inputs and outputs. This figure applies to low-voltage (<30 V) inputs and outputs only.
Figure 1. Maximum wire length for low-voltage Inputs and Outputs by current and wire
size