Firmware Package File - BCPro - Facility Explorer - CH-PCX3733-0 - Field Device - FX-PCX37 Expansion Input/Output Module

PCX3733 Expansion Input/Output Module Installation Guide

Brand
BCPro
Facility Explorer
Product name
FX-PCX37 Expansion Input/Output Module
Document type
Installation Guide
Part number
24-10143-1159
Document revision
C
Version
Revision date
2020-11-11
Language
English

The FX-FCP-0 equipment controller firmware package files are required for CCT to configure and commission the controllers. The firmware package files also allow you to upgrade an existing PCX to the latest firmware release available for that expansion module.

Beginning at CCT Release 13, the firmware package files are orderable separately; they are not included with CCT.

For additional information about the firmware package files, refer to the CCT Installation Instructions (LIT-12011259).