Commissioning the Expansion Modules - BCPro - Facility Explorer - CH-PCX3733-0 - Field Device - FX-PCX37 Expansion Input/Output Module

PCX3733 Expansion Input/Output Module Installation Guide

Product
Controls > Input/Output Controls > FX-PCX37 Expansion Input/Output Module
Document type
Installation Guide
Document revision
C
Version
Revision date
2020-11-11
docpartnumberlabel
Part No.
Part number
24-10143-1159

You commission expansion modules with the Controller Configuration Tool (CCT) software, either via a Zigbee wireless dongle, through MAP 4.2+/BACnet Router (Mobile Access Portal (MAP) Gateway at version 4.2 or above), or in BACnetâ„¢ router mode when connected to an FX supervisory controller . Refer to the Controller Tool Help (LIT-12011147) for detailed information on commissioning expansion modules