The following figure displays the physical features of the expansion module, and the accompanying table provides a description of the physical features and a reference to further information where required.
Callout | Physical feature: description and references |
---|---|
1 |
Binary Output (BO) Terminal Block (see Table 1) |
2 |
Mounting Clip (Three Total) (see Figure 1) |
3 |
Device Address DIP Switch Block (see Setting the device address ) |
4 |
24 VAC, Class 2 Supply Power Terminal Block (see Supply power terminal block) |
5 |
Cover Lift Tab (One of Two) (see Removing the expansion module cover) |
6 |
Sensor Actuator (SA) Bus / Field Controller (FC) Bus Terminal Block (see SA/FC bus terminal block) |
7 |
End-of-Line (EOL) Termination Switch (see Setting the End-of-Line (EOL) switch) |
8 |
Binary Input (BI) Terminal Block (see Table 1) |
9 |
LED Status Indicators |