Wall mount applications - BCPro - Facility Explorer - CH-PCX3733-0 - Field Device - FX-PCX37 Expansion Input/Output Module

PCX3733 Expansion Input/Output Module Installation Guide

Product
Controls > Input/Output Controls > FX-PCX37 Expansion Input/Output Module
Document type
Installation Guide
Document revision
C
Version
Revision date
2020-11-11
docpartnumberlabel
Part No.
Part number
24-10143-1159

About this task

To mount an expansion module directly on a wall or other flat vertical surface, complete the following steps:

Procedure

  1. Pull the two bottom mounting clips outward and ensure they are locked in the extended position.
  2. Mark the mounting hole locations on the wall using the provided dimensions and one of the mount positions, vertical or horizontal. You can also hold the expansion module up to the wall or surface in a proper mount position and mark the hole locations through the mounting clips.
  3. Drill holes in the wall or surface at the marked locations, and insert appropriate wall anchors in the holes (if necessary).
  4. Hold the expansion module in place, and insert the screws through the mounting clips and into the holes (or anchors). Carefully tighten all of the screws.
    Important: Do not overtighten the mounting screws. Overtightening the screws may damage the mounting clips.