Observe the Status LEDs on the front of the expansion module. Table 1 provides LED status indicator information for troubleshooting the expansion module.
LED label | LED color | Normal LED state | Description of LED states |
---|---|---|---|
POWER |
Green |
On Steady |
Off Steady = No Supply Power. The expansion module’s polyswitch/resettable fuse may be open. Check output wiring for short circuits and cycle power to expansion module. On Steady = Power Connected |
FAULT |
Red |
Off Steady |
Off Steady = No Faults On Steady = Device Fault ; This condition may indicate that no application is loaded, that the firmware is mismatched between the controller and the FX-ZFR1811 Wireless Field Bus Router, or (if the controller is in Boot mode) that a Main Code download is required. Blink - 2 Hz = Download or Startup in progress: not ready for normal operation |
SA/FC BUS |
Green |
Blink - 2 Hz |
Blink - 2 Hz = Data Transmission (normal communication) Off Steady = No Data Transmission (N/A - auto baud not supported) On Steady = Communication lost; waiting to join communication ring |
EOL |
Amber |
Off (Except on terminating devices) |
On Steady = EOL switch in ON position Off Steady = EOL switch in Off position |