Application - BCPro - Facility Explorer - CH-PCX3733-0 - Field Device - FX-PCX37 Expansion Input/Output Module

PCX3733 Expansion Input/Output Module Installation Guide

Product
Controls > Input/Output Controls > FX-PCX37 Expansion Input/Output Module
Document type
Installation Guide
Document revision
C
Version
Revision date
2020-11-11
docpartnumberlabel
Part No.
Part number
24-10143-1159

PCX expansion modules expand the number of input/output points connected to either a FX-PCA, FX-PCG, or FX-PCV programmable controller or to an FX Supervisory Controller .

FX-PCX expansion modules operate on an RS-485 BACnet® MS/TP bus and integrate into the web-based FX system.

Note: With Release 10.1 and later of the Controller Configuration Tool (CCT), PCAs, PCGs, or PCVs can be configured to communicate by using either the BACnet MS/TP or the N2 field bus networking protocol. The operation of the PCX is not affected by the selection of the BACnet MS/TP or the N2 protocol in the host controller, when the PCX is connected to the host controller using the SA bus.