Input and output terminal blocks - BCPro - Facility Explorer - CH-PCX2723-0 - Field Device - FX-PCX27 Expansion Input/Output Module

PCX2723 Expansion Input/Output Module Installation Guide

Product
Controls > Input/Output Controls > FX-PCX27 Expansion Input/Output Module
Document type
Installation Guide
Document revision
D
Version
Revision date
2020-11-11
docpartnumberlabel
Part No.
Part number
24-10143-1116

The input terminal blocks are mounted on the bottom of the expansion module and the output terminal blocks are mounted on the top of the expansion module.