Commissioning - BCPro - Facility Explorer - CH-PCX2723-0 - Field Device - FX-PCX27 Expansion Input/Output Module

PCX2723 Expansion Input/Output Module Installation Guide

Product name
FX-PCX27 Expansion Input/Output Module
Document type
Installation Guide
Document revision
D
Version
Revision date
2020-11-11

You commission expansion modules with Controller Configuration Tool (CCT) software through Mobile Access Portal (MAP) Gateway at version 4.2 or above, or in BACnet router mode when connected to a Supervisory Controller. Refer to the Controller Tool Help (LIT-12011147) for detailed information on commissioning expansion modules.