Wall mount applications - BCPro - Facility Explorer - CH-PCX2723-0 - Field Device - FX-PCX27 Expansion Input/Output Module

PCX2723 Expansion Input/Output Module Installation Guide

Brand
BCPro
Facility Explorer
Product name
FX-PCX27 Expansion Input/Output Module
Document type
Installation Guide
Part number
24-10143-1116
Document revision
D
Version
Revision date
2020-11-11
Language
English

About this task

To mount an expansion module directly on a wall or other flat vertical surface, complete the following steps:

Procedure

  1. Pull the two bottom mounting clips outward and ensure they are locked in the extended position, as shown in Figure 1.
  2. Mark the mounting hole locations on the wall using the dimensions in Figure 1 and one of the mount positions shown in Figure 1. You can also hold the expansion module up to the wall or surface in a proper mount position and mark the hole locations through the mounting clips.
  3. Drill holes in the wall or surface at the marked locations, and insert appropriate wall anchors in the holes (if necessary).
  4. Hold the expansion module in place, and insert the screws through the mounting clips and into the holes (or anchors). Carefully tighten all of the screws.
    Important: Do not overtighten the mounting screws. Overtightening the screws may damage the mounting clips.