Mounting features and dimensions - BCPro - Facility Explorer - CH-PCX2723-0 - Field Device - FX-PCX27 Expansion Input/Output Module

PCX2723 Expansion Input/Output Module Installation Guide

Brand
BCPro
Facility Explorer
Product name
FX-PCX27 Expansion Input/Output Module
Document type
Installation Guide
Part number
24-10143-1116
Document revision
D
Version
Revision date
2020-11-11
Language
English

See the following figure for mounting dimensions listed in millimeters and inches. Inches are listed in parenthesis. The following figure also illustrates the DIN rail channel and the mounting clips in an extended position.

Figure 1. Back of expansion module