Features - BCPro - LIT-1900878 - CN-BIG1970-0 - Bulb controller - Modbus Gateway

Modbus Gateway Catalog Page

Product
Network and Communications > Gateways and Routers > Modbus Gateway
Document number
LIT-1900878
Revision date
22/03/2019
  • Efficient gateway for use with the BCPro Workstation to communicate between Modbus RTU or Modbus TCP and BACnet® IP.
  • Support for up to 100 Modbus field devices under a single gateway.
  • Support for the integration to the BCPro Workstation so that gateway configuration can be done using a single login identity.
  • Basic diagnostics provided