An FC bus connects a BACnet Router to CGMs, CVMs, and CH-PC Series Programmable Controllers and other Johnson Controls® or third-party BACnet MS/TP controllers.
Figure 1. Example of an MS/TP Communications Bus

An FC bus supports up to three bus segments that are connected with network repeaters (Figure 1). See Local FC Bus Rules and Specifications for more information.