Baud Rates on the MS/TP Bus - BCPro - LIT-12011908 - General System Information - BCPro System - 4.0

MS/TP Communications Bus for the BCPro System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > BCPro System
Document number
LIT-12011908
Version
4.0
Revision date
2020-03-16

An MS/TP bus can be configured to communicate at one of four different baud rates. All of the devices on an MS/TP bus must communicate at the same baud rate.

The baud rate setting determines the rate at which devices communicate data over the bus. The baud rate settings available on CH-PC devices are 9600 bps, 19.2 kbps, 38.4 kbps, 76.8 kbps, and Auto. The baud rate setting for CH-PC devices is set in the CH-PC software.

Note: The BACnet Standard only requires support for 9600 baud. Some third-party vendor devices might not support all the baud rates supported by the BCPro system. Reducing the baud rate to accommodate these devices affects overall performance.

We recommend setting all MS/TP bus supervisors ( BACnet Routers ) to 38,400.

We recommend setting all CH-PC controllers on the FC bus ( C4-CGMs, C4-CVMs, CH-PCGs, CH-PCAs, CH-PCVs, and CH-PCXs ) to Auto. In the Auto setting, the BCPro devices listen for the bus supervisor to communicate first; the devices then automatically set their baud rate to the bus supervisor’s baud rate. CH-PC controllers ship with a default baud rate setting of Auto.

If you anticipate critical peer-to-peer communication and therefore do not want equipment controllers to wait for the bus supervisor to establish the baud rate, you can specify the baud rate for each device immediately at startup. Choose the baud rate carefully if you use this method, since changing it requires changing each device separately.

Typically, the baud rate setting on bus repeaters and third-party MS/TP devices is configured manually at the device, and the baud rate setting must match the bus supervisor’s baud rate. A third-party device that does not support auto-baud establishes the baud rate for the MS/TP network if the router is not connected. Refer to the manufacturer’s product documentation for information on setting the device’s baud rate.

The BCPro software contains the following two device attributes that relate to the baud rate:

  • Baud Rate Selection allows you to set the baud rate for the device using the Building Configuration Tool (BCT) for Johnson Controls BACnet Routers , or the CCT for C4-CGMs, C4-CVMs, CH-PCGs, CH-PCAs, CH-PCVs, and CH-PCXs .

  • Active Baud Rate allows you to view the baud rate at which the device is communicating on the active bus when Auto baud is selected for the device.

For more information on BCPro system attributes, refer to the BCPro system Help (LIT-12011905) .

The high baud rates capable on MS/TP buses limit the range of wire gauges used on the bus. The baud rate, wire gauge, wire length, and the number of devices are related. Higher baud rates support more devices but require small gauge wire that provides lower capacitance. A lower baud rate may be required to use existing, larger gauge wire that has higher capacitance, but may support fewer devices. We recommend 38,400 baud using 22 AWG stranded wire. This combination provides the best balance between performance and installation sensitivity.

For information on determining wire gauges, wire lengths, and the number of devices supported, see MS/TP Bus Cable Recommendations.