Table 1, Table 2, and Figure 1 provide rules and specifications for the local FC bus.
Category |
Rules/Limits |
---|---|
General |
The BACnet Router can support one FC bus. Check BACnet Router product literature for more details. Note:
An FC port on a BACnet Router can connect to only one bus segment on an FC bus. Only a daisy-chain topology is allowed (no T or Star topology configurations). |
Number of Devices and Bus Segments |
When one or more
non-CH family device is connected on
the FC bus, the device and bus segment limits are as
follows:
he
device and bus segment limits are as follows:
|
Bus segments on an FC bus are connected with repeaters (only). Up to two cascaded repeaters may be applied to an FC bus (to connect three bus segments). |
|
Cable Length for FC Bus and Bus Segments |
When all of the devices connected on the FC bus are
CH-PCGs, CH-PCVs, or CH-PCXs, the cable
length limits (using 22 AWG 3-wire twisted, shielded cable) are
as follows:
When one or more
non-CH
family
TEC26xx Series Thermostat Controllers or
third-party MS/TP device is connected on the FC bus,
the device and bus segment limits are as follows:
Note: Do not place subordinate devices on the FC bus. Subordinate devices on the FC bus are not supported.
|
When using fiber-optic connections: 2,010 m (6,600 ft) between two fiber modems. |
|
Recommended Cable |
22 AWG Stranded, 3-Wire Twisted, Shielded Cable |
EOL Termination |
The EOL switch must be set to On (or an EOL terminator installed) on the two devices located at either end of each bus segment on an FC bus. The EOL switches must be set to Off (or EOL termination disabled) for all other devices on the bus segment on an FC bus. See End-of-Line Termination on Local FC Bus for more information. |
- The recommended cable type provides the best bus performance. See MS/TP Bus Cable Recommendations for information on alternative cable types and lengths that may be used in MS/TP applications.
- If third-party devices are connected to the bus, the cable lengths should be reduced (if necessary) to match the third-party vendor recommendations.
The bus segments on an FC bus are connected using repeaters (only). A repeater has two device connections, which are independent of each other. Each device connection on the repeater is connected to a bus segment just like any other device connection on the segment, and a repeater device connection can be connected at the end of a bus segment or anywhere along the segment. When a repeater device connection is at the end of a bus segment, EOL termination must be enabled on that repeater device connection. See Figure 1 for more examples of repeaters on FC buses.
Category |
Specification |
---|---|
Error Checking |
Message Headers checked using 8-bit Cyclic Redundancy Check (CRC) test. Message data check using 16-bit CRC test. |
Device Addressing |
0–255 (See Device Addressing on the MS/TP Bus for more information.) |
Data Transmission Standard |
RS485 |
Signaling Method |
BACnet® MS/TP |
Signaling Rate |
9600; 19,200; 38,400; or 76,800 baud as selected by bus supervisor. (See Baud Rates on the MS/TP Bus.) |
Transient Immunity |
Meets EN61000-4-4 and EN6100-4-5 requirements for heavy industrial applications. Protected against misapplication of 24 VAC. |
EOL Termination Method |
Integral EOL Termination switch or add-on EOL Terminator module (See End-of-Line Termination on Local FC Bus.) Do not use third-party EOL termination. |
Shield Grounding |
Only one hard ground connection per bus segment when using shielded cable. (See Grounding the MS/TP Bus Cable Shield.) |
Physical Configuration |
Daisy-chained |
Optional Vendor Components |
Repeaters
Note: A repeater is required to support more than 50 devices per
trunk segment or trunk cable segment longer than 1,524 m
(5,000 ft). Only the repeaters listed here provide EOL
termination switching that is compatible with MS/TP.
Transient Eliminator For further information, see Surge Protectors.
Fiber Modem
Note: A DIN rail mounting version of the Model 2110BAC may be
available as Model 2110BAC-DIN. However it does not appear on
the S.I. Tech web site at the time of this writing. Contact S.I.
Tech using contact information on their web site at http://www.sitech-bitdriver.com/index.htm.
|