Commission the devices on the MS/TP bus using the CCT software. Refer to Controller Tool Help (LIT-12011147) for information on commissioning an MS/TP bus application.
Applications and device configurations are downloaded to the hardware from the CCT computer using the Bluetooth Commissioning Converter (FX-BTCVT-1).
Note: The MAP Gateway serves as a replacement for the BTCVT, which
is no longer available for purchase, but continues to be supported.