Excessive Traffic - BCPro - LIT-12011908 - General System Information - BCPro System - 4.0

MS/TP Communications Bus for the BCPro System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > BCPro System
Document type
Technical Bulletin
Document number
LIT-12011908
Version
4.0
Revision date
2020-03-16

SA Bus traffic includes change of value (COV) messages that are issued from inputs located on CH-PCXs and commands issued to outputs located on the CH-PCXs . Excessive traffic is defined as more than 500 COVs per minute or more than 500 commands per minute.

To resolve communication issues associated with excessive SA Bus traffic, reduce the number of COVs to fewer than 500 per minute and the number of commands to fewer than 500 per minute.

Note: The limit of 500 commands per minute is an approximate maximum that assumes a 1 second token loop time. If your network is configured differently, the actual threshold for this problem may vary. For example, if your token loop time is 2 seconds, the maximum is 240. If you reduce traffic on the SA Bus to 500 and still experience this problem, or you are uncertain of your token loop time, we recommend you reduce command traffic to 240.

To find the number of COVs and commands on your SA Bus, see Inputs and COVs and Outputs and Commands. For strategies on reducing traffic on your SA Bus, see SA Bus Traffic Reduction.