Observe the following guidelines to maximize the performance of an MS/TP bus.
|
Guideline |
Description |
|---|---|
|
Limit the Number of Change of Value (COV) Report Rates over the MS/TP Bus |
COV reports account for the highest amount of traffic on the bus. For best performance, keep the COV rate at 200 COVs per minute or fewer for each network. To reduce the COV traffic:
For mapped analog points, where the values are changing frequently, consider the following to limit COV reports:
Note: For some Analog Inputs (AIs), this value cannot be modified.
|
|
Do Not Place Subordinate Devices on the FC Bus |
Subordinate devices on the FC bus are not supported. The SA bus only supports a specific set of subordinate devices. |
|
Carefully Evaluate Third-Party Devices |
Third-party devices can seriously degrade both hardware and software performance depending on their quality and configuration. Consider and configure third-party devices carefully according to the manufacturer’s specifications. |
|
Do Not Add Extra Traffic |
Once the system is configured, commissioned, and running, avoid adding extra traffic to the bus by performing unnecessary auto-discovery operations, downloads, or bus analysis. |
|
Observe the MS/TP Wiring Guidelines |
Follow the wiring rules carefully. The tolerances of the MS/TP bus are tighter than other, slower protocols may be. Improper terminations may result in errors causing serious network degradation. See MS/TP Bus Cable Recommendations. |
|
Check the MS/TP Statistics for Errors |
|
|
Use Default MS/TP Settings |
Avoid changing default MS/TP bus settings, especially settings you may be unfamiliar with. Some parameters set improperly or randomly can cripple the MS/TP bus completely. |