Bus Health Index - BCPro - LIT-12011908 - General System Information - BCPro System - 4.0

MS/TP Communications Bus for the BCPro System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > BCPro System
Document type
Technical Bulletin
Document number
LIT-12011908
Version
4.0
Revision date
2020-03-16

The Bus Health Index is a snapshot of the immediate number of errors on the bus. This index provides a weighted moving average of four MS/TP bus error counters: Framing Errors, Header CRC Errors, Data CRC Errors, and Lost Tokens. The ideal value for the Bus Health Index is zero.

Because the average is reevaluated every 30 seconds, the average gradually returns to zero if no new errors occur. As such, if errors occur only periodically (for example, only when a source of bus interference [such as a welder] is in use), the Bus Health Index may return to zero before you see the value indicate that there are errors. If you suspect that errors are occurring, look at the four error counter attributes. Alternatively, you can trend the Bus Health Index to see when or if it changes during the course of the day.

The Weighted Bus Health Constant attribute is an adjustment factor that determines how quickly the Bus Health Index returns to zero if there are no new errors. The smaller the value of the constant, the slower the index returns to zero.

Typically, the errors indicated by the Bus Health Index are physical bus problems. See Correcting Physical Bus Problems.