Several factors can influence the behavior of the MS/TP bus. In addition, certain problems can affect the bus in multiple ways and have more than one symptom, making the exact diagnosis difficult. For example, duplicate addresses on the bus can degrade performance, make a device go offline, or stop communication completely. Table 1 lists common problems that you should consider when troubleshooting an MS/TP bus. The first row, Multiple Symptoms, lists possible problem causes that can have multiple symptoms.
Symptom |
Possible Causes |
---|---|
Multiple Symptoms |
|
Poor Performance |
|
Devices Go Offline |
|
Device Does Not Come Online |
|