The instructions for configuring the repeater for use with the FC bus require that you perform the following:
-
Set the baud rate to match the FC bus baud rate.
-
Wire the repeater between two segments of the MS/TP bus. If you are using this repeater in a branch, the side with the branch has double the number of wires terminated. See Figure 1.
-
Set the EOL jumpers on the repeater according to Table 1.
For repeater installation instructions and important safety information, refer to the repeater manufacturer’s literature.
Side |
Jumper |
Instructions |
---|---|---|
Side A |
J1 and J2 |
At end-of-line: Install both jumpers over Pins 1 and 2 (EOL In). |
Not at end-of-line: Install both jumpers over Pins 2 and 3 (EOL Out). |
||
Side B |
J3 and J4 |
At end-of-line: Install both jumpers over Pins 1 and 2 (EOL In). |
Not at end-of-line: Install both jumpers over Pins 2 and 3 (EOL Out). |