The 2110BAC modem does not have an EOL jumper. Instead, establish EOL
termination on a 2110BAC modem by properly terminating the FC bus wires to the 9-pin
connector. Soldering the wires to specific pins and soldering two jumper wires
configures the modem as an end-of-line device (see Figure 1, Figure 1, and
Table 1 for more
information).
Note: A DIN rail mounting version of the Model 2110BAC may be available as
Model 2110BAC-DIN. This model would not require soldering the MS/TP wires. However
it does not appear on the S.I. Tech web site at the time of this writing. Contact
S.I. Tech using contact information on their web site at http://www.sitech-bitdriver.com/index.htm.
Do not set the fiber modem as an EOL device on the SA bus.