Routing and Connecting the Fiber Cables - BCPro - LIT-12011908 - General System Information - BCPro System - 4.0

MS/TP Communications Bus for the BCPro System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > BCPro System
Document type
Technical Bulletin
Document number
LIT-12011908
Version
4.0
Revision date
2020-03-16

About this task

To route and connect the fiber cables, follow these steps and see Figure 1:

Procedure

  1. Route the optical fiber in a manner that is required for the application.
  2. Connect the fiber cable from the T (Transmit) output of the modem nearest to the BACnet Router to the R (Receive) input of the modem near the MS/TP devices.
  3. Connect the fiber cable from the T (Transmit) output of the modem near the MS/TP devices to the R (Receive) input on the modem nearest to the BACnet Router.
  4. Plug in the power supply for each modem.
    Figure 1. Connecting the 2110 Modems