Connecting Modems to MS/TP Bus - BCPro - LIT-12011908 - General System Information - BCPro System - 4.0

MS/TP Communications Bus for the BCPro System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > BCPro System
Document number
LIT-12011908
Version
4.0
Revision date
2020-03-16

Connect the MS/TP bus to the 2110BAC modem by soldering the MS/TP wires to pins on the 9-pin connector, which can also configure the modem as an EOL device. To connect the bus, see Setting Termination on Fiber Modems.

Note: A DIN rail mounting version of the Model 2110BAC may be available as Model 2110BAC-DIN. This model would not require soldering the MS/TP wires. However, Model 2110BAC-DIN does not appear on the S.I. Tech web site at the time of this writing. Contact S.I. Tech using contact information on their web site at http://www.sitech-bitdriver.com/index.htm.