Fiber-Optic Modems - BCPro - LIT-12011908 - General System Information - BCPro System - 4.0

MS/TP Communications Bus for the BCPro System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > BCPro System
Document number
LIT-12011908
Version
4.0
Revision date
2020-03-16

You can install the 2110BAC fiber-optic modems in any location on the FC bus. Just as only two repeaters can be cascaded on the FC bus, only two pairs of 2110BAC modems can be cascaded.

The first installation step is to route the optical fiber and connect each modem to the ends of the fiber. The second step is to connect the FC bus on both sides of the modems.