Sensor port - BCPro - Part No. 24-10143-01663 - Field Device - PCV: Programmable VAV Box Controller

CH-PCV1930 VAV Controller Installation Instructions

Brand
BCPro
Product name
PCV: Programmable VAV Box Controller
Document type
Installation Guide
Document number
Part No. 24-10143-01663
Document revision
B
Revision date
2019-03-22
Language
English

The Sensor (SA Bus) port on the bottom of the controller (Figure 1) is an RJ-12, 6-position modular jack that provides a connection for the Mobile Access Portal (MAP) Gateway, the Bluetooth Commissioning Converter (BTCVT), the VAV Balancing Tool, specified network sensors, or other SA Bus devices with RJ-12 plugs. A DIS1710 Local Controller Display can also be connected to the SA Bus port.

Note:
  • Do not use the modular SA Bus port and the terminal block SA Bus simultaneously. Only use one of these connections at a time.
  • The MAP Gateway serves as a replacement for the BTCVT, which is no longer available for purchase, but continues to be supported.

The Sensor port is connected internally to the SA bus terminal block. For more information about Sensor port functions, requirements, and ratings, see Table 1.

Figure 1. Pin number assignments for Sensor (SA Bus) Port on CH-PCV1930