Input and Output terminal blocks - BCPro - Part No. 24-10143-01663 - Field Device - PCV: Programmable VAV Box Controller

CH-PCV1930 VAV Controller Installation Instructions

Brand
BCPro
Product name
PCV: Programmable VAV Box Controller
Document type
Installation Guide
Document number
Part No. 24-10143-01663
Document revision
B
Revision date
2019-03-22
Language
English

The input spade terminals are located on the side of the CH-PCV near the SA Bus terminal block. The output spade terminals are located on the opposite side of the controller near the power supply terminal block. See Table 1 for more information about I/O terminal functions, requirements, and ratings.