LED status and states - BCPro - Part No. 24-10143-01663 - Field Device - PCV: Programmable VAV Box Controller

CH-PCV1930 VAV Controller Installation Instructions

Brand
BCPro
Product name
PCV: Programmable VAV Box Controller
Document type
Installation Guide
Document number
Part No. 24-10143-01663
Document revision
B
Revision date
2019-03-22
Language
English
Table 1. Status LEDs and description of LED states

LED label

LED color

Normal state

Descriptions of LED states

POWER

Green

On Steady

Off Steady = No power

On Steady = Power is supplied by primary voltage

FAULT

Red

Off Steady

Blink - 2 Hz = Download or startup in progress, not ready for normal operation, SA Bus devices offline (such as netsensors)

Rapid blink = SA Bus communications issue

Off Steady = No faults

On Steady = Device fault or no application loaded

SA BUS

Green

Blink - 2 Hz

Blink - 2 Hz = Data transmission (normal communication)

Off Steady = No data transmission (N/A - auto baud not supported)

On Steady = Communication lost; waiting to join communication ring

ETH1

Green

Off

Off Steady = ETH1 is not connected

Blinking = ETH1 connected and communicating