Commissioning Field Controllers - BCPro - Part No. 24-10143-01663 - Field Device - PCV: Programmable VAV Box Controller

CH-PCV1930 VAV Controller Installation Instructions

Brand
BCPro
Product name
PCV: Programmable VAV Box Controller
Document type
Installation Guide
Document number
Part No. 24-10143-01663
Document revision
B
Revision date
2019-03-22
Language
English

To commission the CH-PCV1930 controller, use the following procedure:

  1. Download the control application to the CH-PCV controller using the Controller Configuration Tool (CCT). Refer to the Controller Tool Help (LIT-12011147).
  2. Commission the VAV Box. Refer to the Controller Tool Help (LIT-12011147).
  3. Perform airflow balancing on the VAV box. Refer to the VAV Box Balancing Tool and Network Sensors Technical Bulletin (LIT-12011659).
  4. Perform commissioning checkout procedures. Refer to the Controller Tool Help (LIT-12011147).
Note:
  • The MAP Gateway serves as a replacement for the BTCVT, which is no longer available for purchase, but continues to be supported.