Workstation Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab and the Diagnostics tab.

Click the attribute name in the table for a description of the attribute.

Table 1. Workstation Device Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Flags 1

Initial Value

Values/Options/Range1

APDU Retries 2

Number

CW

4

2–10

APDU Segment Timeout 2

Number

CW

10,000

1,000–65,535

Units = milliseconds

APDU Timeout 2

Number

CW

10,000

1,000–65,535

Units = milliseconds

Archive Date

Date

     
BACnet IP Port 2

Number

CW

47,808

0–65,535

Device Object Identifier

Number

C

B

0 - 4194303

DHCP Enabled

True or False

CW

True (1)

0 = DHCP disabled,

1 = DHCP enabled

Duplicate References

List

     
Enabled Audit Level

One from a list of values

CW

Audit Level 2 (1)

See the attribute description for details on the Enabled Audit Level.

Range = 1–4 with 5 Audit Levels

Level 1 (N/A) User Action

Level 2 (1) Critical System Events

Level 3 (2) Application

Level 4 (3) Non-critical System Events

Level 5 (4) Diagnostic

Firmware Version

Text

     
Host Name

Text

     
Internode Comm Timer

Number

CW

120

Range = 5–255

Local Date

Date

     
Local Time

Time

     
Max APDU Length 2

Number

CW

1,024

128–65,535

Units = bytes

Max Message Buffer

Number

CW

994

98–65,535

Units = bytes

Model Name

Text

 

CH-BCM100-0

 
Network Address 2

Number

CW

1,001

0–65,535

Unbound References

List

     
Table 2. Workstation Device Object Attributes - Diagnostic Tab

Attribute Name

Data Type

Flags 3

Initial Value

Values/Options/Range3

Average Intermittent Failure Period

List

   

IP address and Value

Units = seconds

BACnet Broadcast Receive Rate

Number

   

Units = Per Minute

BACnet Routed Messages Rate

Number

   

Units = Per Minute

COV Rcv Rate

Number

   

Units = Per Minute

COV Tx Rate

Number

   

Units = Per Minute

Detection Interval

Number

   

Units = seconds

Maximum Intermittent Failure Period

List

   

IP address and Value

Units = seconds

Network Tolerance

One from a list of values

CW

Low

Uses Error Tolerance set.

Low, Medium, High

Object Count

Number

     
Object Memory Usage

Real value

   

Units = %

Display Precision = 1.0

COV Increment = 1.0

Transport Failure Rate

List

   

IP address and Value

Units = Failures Per Day

Note: If you write the value of this attribute, you must restart the Workstation for the new settings to take effect.
1 C - Configurable, N - Value Not Required, Q - BACnet Required, W - Writable
2 If you write the value of this attribute, you must restart the Workstation for the new settings to take effect.
3 C - Configurable, N - Value Not Required, Q - BACnet Required, W - Writable