Paste Item Wizard - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Menu Selection: Edit > Copy > Paste.

Copies an item from the navigation tree such as an AV object, field device, or supervisory device and pastes it into another location in the navigation tree in the BCT.

Tip: You can copy an item and paste it into another equivalent node in the navigation tree or you can copy an item and paste it into the same node on the tree, but you must select a new name for the item. For example, you can copy a Router from Site 1 and paste it into Site 1 or Site 2 if you rename it Router 2. You cannot paste a Router under another Router, field device, or object (you must paste it under a Site).
Tip: When you copy and paste a field point, the new point automatically receives a unique hardware address.