Passthru Wizard - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Modes: Available in online and offline modes only

Menu Selection: Tools > Field Device Tools

Accesses CCT.

Tip: You must have CCT and the BCT installed on the same computer that is running the CCT passthru. To use the CCT in Ethernet passthru mode, open CCT from the Tools > Field Device Tools > CCT (MSTP) menu option.
Tip: The Passthru wizard does not always appear when you are connected to the BCPro Workstation online if you are already logged on to the site. The selected tool loads automatically after selecting it from the Tools menu.
Tip: On the Passthru Site Login screen of the wizard, enter your username and password as defined by your User Profile. By default, your username and password should automatically appear. If desired, click Test Login to check if your login parameters are valid to access the tools.