Open Archive Wizard - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Menu Selection: Item > Open Archive

Opens an existing archive database in the BCT.

Archives appear locked when someone else is accessing that archive. If a user has an archive open and closes the UI incorrectly (not clicking the Exit or Logout button), the database appears locked to all users with a different username/password. To reverse the lock, a user with the same username/password as the user who closed the UI incorrectly must open that archive, then close the UI properly.