Insert Site Wizard - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Menu Selection: Insert > Site

Inserts a site into the archive database in the BCT.

Tip: The Create Device? dialog box appears after inserting a site asking if you want to create a device in the site. Selecting Device and clicking OK invokes the Insert Device wizard. Selecting BCPro Server and clicking OK invokes the Insert BCPro Server wizard. Select None and OK if you do not want to add a device at this time.
See one of the following sections for more information: