Menu Selection:
Inserts one of the following types of field points into a field device under an
integration:
-
BACnet
All field points listed for the N2 trunk plus Analog Value Object (AV), Binary Value Object (BV), Calendar Object, Multistate Value Object (MV), Schedule Object
-
MS/TP Field Bus Integration
Analog Input Object (AI), Analog Output Object (AO), Analog Value Object (AV), Binary Input Object (BI), Binary Output Object (BO), Binary Value Object (BV), Multistate Value Object (MV), Calendar Object, Schedule Object
Tip: On the Select Definition Mode screen, select Assisted Point Definition to
automatically discover existing points on the network.
Tip: Or on the Select Definition Mode screen, select Manual Point Definition.
Tip: Select the Hardware tab on the Configure screen for further configuration.
See one of the following sections for more information: