Insert Object Wizard - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Insert Object wizard inserts one of the following object types:

  • Insert Object - AV

    Menu Selection: Insert > Object

    Inserts an Analog Value Object into the site.

  • Insert Object - BV

    Menu Selection: Insert > Object

    Inserts a Binary Value Object into the site.

  • Insert Object - Calendar

    Menu Selection: Insert > Object

    Inserts a Calendar Object into the site.

    See Scheduling for more information on applying scheduling capabilities.

  • Insert Object - Global Data

    Menu Selection: Insert > Object

    Inserts a Global Data Sharing Object into the site.

  • Insert Object - Interlock

    Menu Selection: Insert > Object

    Inserts an Interlock Object into the site.

    Note: On the Configure screen, click the Interlock Definition and Action Tables tabs for further configuration.

    Tips for the Interlock Definition tab of the Configure screen:

    • Click the Add button to add items to the list from the Select Item dialog box.

    • Click the check box next to an item in the list and click Delete to remove the item from the list.

    • Select the type of logic to use for the items in the list from the Logic menu. See the Interlock Object’s Logic attribute description for the types of logic.

    Tips for the Action Tables tab of the Configure screen:

    • Check the All Commands Priority check box if you wish to use the same priority for all commands in the action tables. Clear the All Commands Priority check box to enable individual priority selection for the commands in the action tables.

    • For the Actions for Condition: True and Actions for Condition: False tables, click the Add button to add items to the table from the Select Item dialog box.

    • For the Actions for Condition: True and Actions for Condition: False sections, click the check box next to an item in the table and click Delete if you want to remove the item from the table.

  • Insert Object - MV

    Menu Selection: Insert > Object

    Inserts a Multistate Value Object into the site.

  • Insert Object - Multiple Command

    Menu Selection: Insert > Object

    Inserts a Multiple Command Object into the site.

    Note: On the Configure screen, click the Action Tables tab for further configuration.
    Note: Select or enter the desired value for the Relinquish Default. Edit the States Text and Number of States attributes on the Focus tab.
    Note: Check the All Commands Priority check box if you wish to use the same priority for all commands. Clear the All Commands Priority check box to enable individual priority selection for the commands.
    Note: For each of the Actions for Condition (State 0 - State N) tables, click the Add button to add items to the table from the Select Item navigation tree.
    Note: For each of the Actions for Condition (State 0 - State N) tables, click the check box next to an item in the table and click Delete to remove the item from the table.

    See the Multiple Command Object section for more information.

  • Insert Object - Schedule

    Menu Selection: Insert > Object

    Inserts a Schedule Object into the site.

    See Scheduling.

  • Insert Object - Signal Select

    Menu Selection: Insert > Object

    Inserts a Signal Select Object into the site.