Menu Selection:
Integrates the following types of buses or networks into the BCPro system:
- BACnet - Inserts a BACnet integration into the BCPro Workstation.
- Field Bus - Inserts an MS/TP network integration for the BCPro Workstation.
- VND Integration - Inserts a vendor integration into the BCPro Workstation.
Note: Select the Hardware tab (if it appears) on the Configure screen for further configuration.
After adding an integration, you can select the integration in the navigation tree and click add existing devices and points under the integration.
See one of the following sections for more information: