About this task
Menu Selection:
Inserts one of the following types of field device objects under the selected integration:- BACnet Integration - BACnet Integration Object (Non-FEC BACnet Device)
- MS/TP Field Bus Integration - MS/TP Field Bus Integration Object (FEC Family BACnet Device) BACnet Device Object (Non-FEC BACnet Device)
- VND Controller (Vendor) - 3rd party vendor controller, offered through SIS
To insert a field device select the menu selection: