Insert Device Wizard - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Menu Selection: Insert > Device

Inserts a BACnet Router or Modbus Gateway device into the archive database in the BCT.

On the Configure screen of this wizard, click any tabs that may appear for further device configuration.

See one of the following sections for more information: