Insert BCPro Server Wizard - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Menu Selection: Insert > BCPro Server

Inserts a BCPro server (BCPro Workstation) into the archive database in the BCT.

Tip: The BCPro server you add to the site becomes the Site Director. The Site Director coordinates all Web browser communication to the BCPro network. You can only have one Site Director per site.
Tip: On the Configure screen, select each tab for further configuration options.

See Workstation Device Object for more information.