Extension Wizard - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Menu Selection: Actions > Show Extensions (menu option is available only when an item that supports extensions is selected)

Adds features to an item. The only two extension types supported in the BCPro system include:
  • Resource File - Adds a resource file to a field device or integration, if supported.
  • Trend - Adds trending capabilities to an item.

See the Extensions section.